Linear Move
| Description |
The Linear Move command behaves in a similar way to the existing Move To node but supports Motions Profiles. This command creates a movement that is a direct line from point A and point B. It moves the Tool Center Point (TCP) linearly between waypoints. This means that each joint performs a more complicated motion to keep the tool on a straight line path.
|
|
To access Linear Move command |
|
|
|
|
| Using the Move Here button |
The Move Here button is seen in Linear Move and Joint Move commands. This feature enables you to move to the position of a waypoint directly from the program tree. Pressing the Move Here button opens the Move robot into position dialog. The button is visible when the waypoint has been taught and is only enabled when the robot status is in Normal or Reduced mode.
|
| Motion Profile labels on Move Nodes |
All Move-related command nodes in the program tree display the Motion Profile associated with each node. This feature enables users to see the selected Motion Profile on a Move node. This feature is implemented on the following command nodes: Move nodes with Custom motion profile will display the values for the speed and acceleration instead of Motion profile. |
|
|
|
| Movement setting |
|
| Reference setting |
|
| Transform setting |
|
|
Blend setting |
|