Halt

Description

The Halt command allows you to stop the robot at that location.

 

To access the Halt command

  1. Go to the main program screen. See Command Nodes.

  2. Tap the Halt icon in the Commands toolbox.

    You see a notification under the chosen program: "Program execution stops at this point."