Shared Applications in System Manager
| Description |
An Application contains robot configuration and safety settings, such as equipment, end effectors, application variables, and safety parameters. From PolyScope X 10.14, a single Application can be shared by multiple programs. When you change settings in a shared Application, every program linked to that Application uses the updated configuration. Manage Applications and their linked programs from the Programs tab in System Manager.
|
| Programs tab layout |
On the Programs tab, Applications and programs are shown in a unified accordion structure:
|
| Application context menu |
Open the Application context menu to access:
|
| Program actions |
From a program's context menu you can:
When creating a new program, use the Application dropdown to link the program to an existing Application or create a new one. Changes to a shared Application affect all programs that reference it. Verify program behavior after linking or changing Applications.
|