Duplicate Program

Description

Duplicate creates a copy of a program. You can set the name of the new program and choose which Application the duplicated program uses. The dialog is the same as when creating a new program.

 

To duplicate a program
  1. In System Manager, on the Programs tab, select the program you want to duplicate.

  2. Open the program context menu and tap Duplicate.

  3. Enter a name for the new program.

  4. In the Application dropdown, select the Application the duplicated program should use, or choose Create New to create a new Application.

  5. Tap Confirm.