Delete Application
| Description |
You can delete an Application from the Programs tab in System Manager when it is no longer needed. Deletion rules depend on whether programs are still linked to the Application.
|
| Delete Application with linked programs |
If you try to delete an Application that still has programs linked to it, a dialog informs you that you must reassign or delete the linked programs first.
|
| Delete Application with no linked programs |
|
| Delete last program linked to an Application |
When you delete the last program linked to an Application, a dialog asks whether you also want to delete the Application. You can delete both the program and the Application in one step, or delete only the program and keep the Application.
|