Duplicate Application

Description

Duplicate Application creates a copy of an Application's settings. Only the Application is duplicated — programs linked to the original Application are not duplicated.

 

To duplicate an Application
  1. In System Manager, on the Programs tab, open the context menu for the Application you want to duplicate.

  2. Tap Duplicate.

  3. Enter a name for the duplicated Application.

  4. Confirm. The new Application appears in the list with a copy of the source Application settings.