Load Program without Safety Password

Description

This feature lets you load programs without repeatedly entering the Safety Password, while ensuring that only approved safety configurations can be applied. This improves usability without compromising safety.

 

User benefit

These are the benefits of this feature:

  • You can load programs without entering the safety password.

  • You only need the safety password when you modify or apply unapproved safety configurations.

  • New programs use the default safety checksum . You must enter the safety password to create a new safety configuration.

  • You can create programs by copying settings from a loaded program or duplicating an existing program without entering the safety password.

    As in PolyScope 5, approved safety configurations are stored in each program or application.

 

Safety checksum (CCCC)

PolyScope X displays the safety checksum for the currently loaded program. is the default checksum for the default safety configuration.

In PolyScope X, you see the safety checksum in the Sidebar.