Move Into Contact

Description

The Move Into Contact Smart Skill moves the robot in the TCP +Z direction until it reaches a contact point. The robot then retracts by the Retract Distance. The default retract distance is 0 mm.

Move Into Contact Smart Skill

 

Function

You can configure Force, Velocity, Acceleration, Maximum Distance, and Retract Distance.

The Smart Skill zeroes the force/torque sensor at the start and moves along TCP +Z.

Move Into Contact Dialog