Toggle Output

Description

The Toggle Output Smart Skill toggles a configured digital output, for example when you set up or teach a gripper.

Toggle Output Smart Skill

 

Function

This Smart Skill toggles the configured digital output to HIGH or LOW. The setting page lets you select the digital output to toggle. In Teach Mode, you can also insert a Set node. You do not need a Three-Position Enabling Device (3PE) when you run this Smart Skill from the Smart Panel.

Control Box I/O and Tool I/O Toggle Output Selection