Boot Robot Using UR Disk Utility
| Description |
UR Disk Utility is a pre-boot tool for managing robot images and the data on the robot. UR Disk Utility can only use a USB drive to manage robot images. Other types of storage media are not supported.
You can use UR Disk Utility to install a robot image, create or restore a backup of the robot disk, or erase the robot disk. Install, restore, and erase operations overwrite data on the robot disk. Back up any data that you want to keep before you continue.
|
| Install without a Teach Pendant |
UR Disk Utility can install PolyScope X without a Teach Pendant (TP7). If no Teach Pendant is attached to the Control Box and the storage on the Control Box is blank, you can use UR Disk Utility to install PolyScope X.
Make sure that the storage is blank.
PolyScope X is now installed.
|
| Start the robot with UR Disk Utility |
To start UR Disk Utility:
|
||
| Main screen |
Do not remove the UR Disk Utility USB or turn off the robot while an operation is in progress.
|
Install Robot
| Description |
Use Install Robot to install a compatible robot image from the data partition of the UR Disk Utility USB. Insert the UR Disk Utility USB into the Control Box, then start UR Disk Utility. When you copy a robot image from your PC to the UR Disk Utility USB, you do not need to modify the image file. Installing a new image overwrites all data on the robot.
|
| Install Image |
Before the installation starts, select Cancel to return to the main screen without changing the robot disk.
|
| Automatic installation |
If the robot disk is blank and the UR Disk Utility USB contains one compatible robot image, the installation screen can open automatically and display a countdown. Select Start Installation to start immediately, or select Cancel to stop the countdown and return to the main screen. You can only install images inside the installer folder in the UR Disk Utility USB, which also contains a file named autoinstall. In this file, you can configure which image to install first during an automatic installation. If you delete the autoinstall file, automatic installation does not work.
For a comprehensive guide to using UR Disk Utility in PolyScope X, see Boot Robot Using UR Disk Utility.
|
Clone Robot
| Description |
Use Backup Robot to create an image of the robot's internal storage on the data partition of the UR Disk Utility USB. You can use this image to restore the robot to the saved state. Make sure that the UR Disk Utility USB has enough free space for the backup. Do not remove the UR Disk Utility USB drive while the backup is in progress. Rules for naming the file:
|
| Backup Robot |
Before the backup starts, select Cancel to return to the main screen without creating a backup. A robot backup is for backup and recovery. Do not use Backup Robot to manage software across a fleet of robots.
|
Restore Robot
| Description |
Use Restore Backup to restore a backup image from the UR Disk Utility USB to the robot disk. Restoring a backup image overwrites the robot disk. All current data on the robot is lost.
|
| Restore Backup |
Before restoring starts, select Cancel to return to the main screen without changing the robot disk.
|
Erase Robot
| Description |
Use Erase Robot to erase all data from the robot disk. Erase the disk when decommissioning the Control Box or before returning a compatible Control Box to removable-storage operation. All data is erased. The robot cannot start from the robot disk after the erase operation.
|
| Erase Robot |
Before erasing starts, select Cancel to return to the main screen without changing the robot disk. If you start the robot again with the UR Disk Utility USB inserted while the robot disk is blank, automatic installation may start.
|