Align to Plane

Description

The Align to Plane Smart Skill orients the TCP to a surface. It touches 3 points on the surface (the default) and computes the orientation of the plane. The contact points lie on a circle with a default radius of 50 mm. For creating a new frame from a surface, see Frames.

 

 

 

 

Function

You can configure Radius, Push Force, Number of Plane Points, Maximum Distance, Velocity Pressure Downwards, Velocity approaching touch up point, and Velocity Move.

The direction defaults to TCP +Z.

Align to Plane Dialog