Add Move Node

Description

The Add Move Node Smart Skill inserts a move node at the current arm position. It is deactivated by default.

Add Move Node Smart Skill

 

Function

You can insert a Joint Move or Linear Move node after the selected program node, using the current arm position, frame, TCP, and Motion Profile. You do not need a Three-Position Enabling Device (3PE) when you run this Smart Skill from the Smart Panel.

Joint Move and Linear Move Selection