Custom

Description

Custom is a user-authored Smart Skill that runs application-specific logic, typically a main program function.

Custom Smart Skill

 

Function

  1. Tap the kebab icon for Custom and enable this Smart Skill.

  2. This Smart Skill executes a linked function or a generated script. Tap + Create Smart Skill so you do not need to duplicate an existing skill.

  3. You can map this Smart Skill to a Smart Panel button or a TP7 button.

  4. In Teach Mode, you can insert a CALL_FUNCTION node.

    Functions Drop-down Menu