Home

Description

The Home Smart Skill moves the robot to a saved home position. You define that position in the Smart Skills Application application, and you can move to it from the Smart Skills tab. The position is also available as a waypoint.

The upright zero position is the default. Reset deletes the saved pose after you confirm.

Home Smart Skill

 

 

Function

The target pose is drawn as a ghost robot. Opening or leaving Home does not change the Preview toggle.

Home Dialog Showing a Ghost Robot