set_flag(n, b)

Flags behave like internal digital outputs. They keep information between program runs.

Parameters

n: The number (id) of the flag, integer: [0:31]

b: The stored bit. (boolean)

Example command: set_flag(1,True)

  • Example Parameters:
    • n is flag number 1
    • b = True will set the bit to True