get_digital_out(n)
Deprecated: Get digital output signal level
Parameters
n: The number (id) of the output, integer: [0:9]
Return Value
boolean, The signal level.
Deprecated: The get_standard_digital_out and get_tool_digital_out replace this function. Ports 8-9 should be changed to 0-1 for the latter function. This function might be removed in the next major release.
Note: For backwards compatibility n:8-9 go to the tool digital outputs.
Example command: get_digital_out(1)
- Example Parameters:
- n is digital output 1
- Returns True or False
- n is digital output 1