get_configurable_digital_out(n)

Get configurable digital output signal level

See also get_standard_digital_outand get_tool_digital_out.

Parameters

n: The number (id) of the output, integer: [0:7]

Return Value

boolean, The signal level.

Example command: get_configurable_digital_out(1)

  • Example Parameters:
    • n is configurable digital output 1
      • R'eturns True or False