read_input_integer_register(address)
Reads the integer from one of the input registers, which can also be accessed by a Field bus. Note, uses it’s own memory space.
Parameters
address: Address of the register (0:47)
Return Value
The value held by the register [-2,147,483,648 : 2,147,483,647]
Note: The lower range of the integer input registers [0:23] is reserved for FieldBus/PLC interface usage. The upper range [24:47] cannot be accessed by FieldBus/PLC interfaces, since it is reserved for external RTDE clients.
>>> int_val = read_input_integer_register(3)
Example command: read_input_integer_register(3)
- Example Parameters:
- Address = input integer register 3