get_flag(n)

Flags behave like internal digital outputs. They keep information between program runs.

Parameters

n: The number (id) of the flag, integer: [0:31]

Return Value

Boolean, The stored bit.

Example command: get_flag(1)

  • Example Parameters:
    • n is flag number 1
      • Returns True or False