set_configurable_digital_out(n, b)

Set configurable digital output signal level

See also set_standard_digital_out and set_tool_digital_out.

Parameters

n: The number (id) of the output, integer: [0:7]

b: The signal level. (boolean)

Example command: set_configurable_digital_out(1,True)

  • Example Parameters:
    • n is configurable digital output 1
    • b = True