read_input_float_register(address)
Reads the float from one of the input registers, which can also be accessed by a Field bus. Note, uses it’s own memory space.
Parameters
address: Address of the register (0:47)
Return Value
The value held by the register (float)
Note: The lower range of the float input registers [0:23] is reserved for FieldBus/PLC interface usage. The upper range [24:47] cannot be accessed by FieldBus/PLC interfaces, since it is reserved for external RTDE clients.
>>> float_val = read_input_float_register(3)
Example command: read_input_float_register(3)
- Example Parameters:
- Address = input float register 3