ft_rtde_input_enable(enable, sensor_mass=0.0, sensor_measuring_offset=[0.0, 0.0, 0.0], sensor_cog=[0.0, 0.0, 0.0])
This function is used for enabling and disabling the use of external F/T measurements in the controller. Be aware that the following function is impacted:
force_modescrew_drivingfreedrive_mode
The RTDE interface shall be used for feeding F/T measurements into the
real-time control loop of the robot using input variable
external_force_torque of type VECTOR6D. If no other RTDE
watchdog has been configured (using script function
rtde_set_watchdog), a default watchdog will be set to a 10Hz
minimum update frequency when the external F/T sensor functionality
is enabled. If the update frequency is not met the robot program will
pause.
Parameters
enable: enable or disable feature
(bool)
sensor_mass: mass of the sensor in
kilograms (float)
sensor_measuring_offset: [x, y, z] measuring offset of the
sensor in meters relative to
the tool flange frame
sensor_cog: [x, y, z] center of gravity of the
sensor in meters relative to
the tool flange frame
Notes:
This function replaces the deprecated
enable_external_ft_sensor.
The TCP Configuration in the installation must also include the weight and offset contribution of the sensor.
Only the enable parameter is required; sensor mass,
offset and center of gravity are optional (zero if
not provided).
Example command:ft_rtde_input_enable(True, 1.0, [0.1, 0.0,
0.0], [0.2, 0.1, 0.5])
- Example Parameters:
- enable -> Enabling the feed of an external F/T
measurements in the controller.
- sensor_mass -> mass of F/T sensor is set to 1.0 Kg.
- sensor_measuring_offset -> sensor measuring offset is set to [0.1, 0.0, 0.0] m from the tool flange in tool flange frame coordinates.
- sensor_cog -> Center of Gravity of the sensor is set to x=200 mm, y=100 mm, z=500 mm from the center of the tool flange in tool flange frame coordinates.
ft_rtde_input_enable(True, 0.5)- Example Parameters:
enable S{rarr} Enabling the feed of an external F/T measurements in the controller.
sensor_mass S{rarr} mass of F/T sensor is set to 0.5 Kg.
Both sensor measuring offset and sensor's center of gravity are zero.
@example:
C{ft_rtde_input_enable(False)}Disable the feed of external F/T measurements in the controller (no other parameters required)
- Example Parameters:
- enable -> Enabling the feed of an external F/T
measurements in the controller.