modbus_reset_connection(connection_id, is_blocking=True)
Tear down, and reconnect all signals to remote device. By default it will block as long as there are errors in the connection.
>>> modbus_reset_connection("172.140.17.11")
Parameters
connection_id: A string specifying the IP address of the modbus unit to which the modbus signal is connected. The IP can not be empty.
Example command: modbus_reset_connection("172.140.17.11")
Example Parameters:
-
connection_id = 172.140.17.11
-
is_blocking = True
-