Digital Input

Description

The Digital Input field ranges from DI 0 to DI 7.

 

To access Digital Input
  1. Tap DI 0, and the Name and Action Preset fields appear.

  2. In the Name field, create a name and Confirm. The new name can now be seen in the communication screen.

     

     

  3. Repeat steps 3 onward of Configurable Input for DI 1 to DI 7.