Tool IO
| Description |
Tool IO monitors and sets the live IO signals from/to the control box.
|
| To access Tool IO |
Tap Tool IO on the left panel. You can see the editable fields of Tool Input and Tool Output on the right.
|
|
URCaps in Control dropdown |
The Controlled By dropdown field allows user to select a URCap that can control the tool settings. If a URCap is installed that has this capability, it will be displayed in the list. Follow here on how to install a URCap. When selected, the URCap will be responsible for the following settings:
Upon selection of a URCap, any controls related to the above settings will be disabled. The new settings will be applied when an entry is selected in the dropdown, when the program is loaded, and when the program is played.
|