Tool Input

Description

The Tool Input is composed of four fields:

  • DI 0

  • DI 1

  • AI 0

  • AI 1

 

To access Tool Input

  1. Tap DI 0, and the Name and Action Preset fields appear.

  2. In the Name field, create a name and Confirm.

  3. Tap the Action Preset field and select from the five available choices.

  4. Repeat steps 1–3 for DI 1.

  5. Tap AI 0. A Name and Domain fields appear.

  6. In the Name field, create the name you prefer.

  7. Tap the Domain field, and you can choose either Current or Voltage.

  8. Repeat steps 5–7 for AI 1.