Analog Output

Description

Analog output has two fields for AO 0 and AO 1. As with analog input, it can be set to 4–20 mA.

 

To access Analog Output

  1. Tap the purple slider of each field to adjust the current or voltage settings.

  2. Tap AO 0.

  3. In the Domain field, you can choose either Current or Voltage.

  4. Tap the Action Preset field, and eight choices are available:

    • None

    • Min when not running

    • Max when not running

    • Max when running, Min when stopped

    • Min on unscheduled stop

    • Min on unscheduled stop, otherwise Max

    • Max when drive power is on, otherwise Min

    • Min when drive power is on, otherwise Max

 

  1. Choose the pertinent action preset. The purple slider reflects the action preset you choose.

  2. Tap AO 1 and repeat steps 3–5.

    By selecting the last two action preset, the Min/Max value of signals will be changed when power is OFF/ON.