set_tool_digital_out(n, b)
Set tool digital output signal level
For g-Series: Replaced by io_set(alias, value). Use labels such as "T0_DO0". Performance flange also has T1_DO0–T1_DO3.
See also set_configurable_digital_out and set_standard_digital_out.
Parameters
n: The number (id) of the output, integer: [0:1]
b: The signal level. (boolean)
Example command: set_tool_digital_out(1,True)
- Example Parameters:
- n is tool digital output 1
- b = True