get_tool_digital_in(n)
Get tool digital input signal level
g-Series: Replaced by io_get(alias). Use labels such as "T0_CI0". Performance flange also has Smart Panel inputs T1_DI0–T1_DI2 and T1_CI0, T1_CI1.
See also get_configurable_digital_in and get_standard_digital_in.
Parameters
n: The number (id) of the input, integer: [0:1]
Return Value
boolean, The signal level.
Example command: get_tool_digital_in(1)
- Example Parameters:
- n is tool digital input 1
- Returns True or False
- n is tool digital input 1