get_configurable_digital_in(n)
Get configurable digital input signal level
For g-Series: Replaced by io_get(alias). Use labels such as "CB_CI0". CB7 supports CB_CI0–CB_CI15.
See also get_standard_digital_in and get_tool_digital_in.
Parameters
n: The number (id) of the input, integer: [0:7]
Return Value
boolean, The signal level.
Example command: get_configurable_digital_in(1)
- Example Parameters:
- n is configurable digital input 1
- Returns True or False
- n is configurable digital input 1