get_standard_analog_out(n)

Get standard analog output signal level

For g-Series: Replaced by io_get(alias). Use labels such as "CB_AO0".

Parameters

n: The number (id) of the output, integer: [0:1]

Return Value

float, The signal level in Amperes, or Volts

Example command: get_standard_analog_out(1)

  • Example Parameters:
    • n is standard analog output 1
      • Returns value of standard analog output #1