set_standard_digital_out(n, b)
Set standard digital output signal level
g-Series: Replaced by io_set(alias, value). Use labels such as "CB_DO0".
See also set_configurable_digital_out and set_tool_digital_out.
Parameters
n: The number (id) of the output, integer: [0:7]
b: The signal level. (boolean)
Example command: set_standard_digital_out(1,True)
- Example Parameters:
- n is standard digital output 1
- f = True