get_analog_in(n)

Deprecated: Get analog input signal level

For g-Series: Replaced by io_get(alias).

Parameters

n: The number (id) of the input, integer: [0:3]

Return Value

float, The signal level in Amperes, or Volts

Deprecated: The get_standard_analog_in and get_tool_analog_in replace this function. Ports 2-3 should be changed to 0-1 for the latter function. This function might be removed in the next major release.

Note: For backwards compatibility n:2-3 go to the tool analog inputs.

Example command: get_analog_in(1)

  • Example Parameters:
    • n is analog input 1
      • Returns value of analog output #1