get_tool_digital_out(n)
Get tool digital output signal level
g-Series: Replaced by io_get(alias). Use labels such as "T0_DO0". Performance flange also has Smart Panel outputs T1_DO0–T1_DO3.
See also get_standard_digital_out and get_configurable_digital_out.
Parameters
n: The number (id) of the output, integer: [0:1]
Return Value
boolean, The signal level.
Example command: get_tool_digital_out(1)
Example Parameters:
n is tool digital out 1
Returns True or False