get_power_output(alias)
Unified I/O. Introduced at SW 10.15 and 5.26. This script is backward compatible with all previous SW and HW versions.
Returns the voltage set on the tool power output.
See also set_power_output(alias, voltage) and I/O labels.
Parameters
alias: The symbolic name of the pin (string). It can represent one of the tool power outputs.
Return Value
The voltage set on the selected tool power output.
Example command: v_gripper = get_power_output("T2_V")
- Example Parameters:
- Read the voltage applied to the T2 4-pin M8 tool connector:
v_gripper = get_power_output("T2_V")
- Read the voltage applied to the T2 4-pin M8 tool connector: