set_standard_analog_out(n, f)

Set standard analog output signal level

g-Series: Replaced by io_set(alias, value). Use labels such as "CB_AO0".

Parameters

n: The number (id) of the output, integer: [0:1]

f: The relative signal level [0;1] (float)

Example command: set_standard_analog_out(1,1.0)

  • Example Parameters:
    • n is standard analog output port 1
    • f = 1.0, that corresponds to 10V (or 20mA depending on domain setting) on the output port