Three Position

Description

Manual high speed allows both tool speed and elbow speed to temporarily exceed 250 mm/s. It is only available when your robot is on manual mode and a three-position enabling device is configured.

If there is no interaction with the three-position enabling device in five minutes, increased values will be reset to 250 mm/s.

 

To access Three Position
  1. On the left panel, tap Three Position.

  2. Tap Unlock on the upper right side of the main screen.

  3. Enter the safety password and Confirm.

  4. On the central panel, slide on the button to Allow manual high speed.

  5. Tap Apply on the upper right side of the main screen.