Hardware
| Description |
The Hardware section allows users to select the type of Teach Pendant (TP) connected to their robot. Available options are:
For safety reasons, the robot will not start if the selection does not reflect the connected hardware.
|
| Purpose of None option |
The None option supports setups where a Teach Pendant is not required or physically present, enabling more streamlined and flexible deployments, especially in automated or remote-controlled environments. It gives users three key benefits:
|
| To access None |
|
|
|
|