Restoration of Recovered Image Files
| Description |
To restore recovered robot image files, you need Linux file system support, as in data recovery.
|
|
Re-imaging using Linux command |
This is an optional process. Use this procedure if you successfully recovered and re-imaged the robot file.
To re-image a recovered file, use a Linux command such as:
sudo dd if="/path/to/ursys-CB5.0-5.24.0-build12.19.432-secure.img" of=/dev/sdb bs=4M status=progress
Where:
|