Files to Download

Description

This section provides three links to download and install the following:

  1. A free and open-source tool to create bootable USB drives.

  2. Universal Robots robot image based on the robot arm size.

  3. Software for managing a Linux file system. For details, see Recovery of Data.