--

Complete your cobot

Browse products to use with your cobot. Create a complete automation solution with end effectors, software, seventh axis and more.
  • Category
    1
  • Applications
    3
  • Product Type
  • Compatibility
  • Region

10 products

Showing

12

36

CNC Machine Tending
App Kit
Robotiq

CNC Machine Tending

Today’s manufacturers want to automate manual tasks with robots, but getting robots up and running is complex, expensive, and can leave you feeling overwhelmed. At Robotiq, we believe robots should simplify your life, not make it more complicated. Working with manufacturers globally (and being one ourselves!), we understand the challenges of maintaining quality, delivering on time, and keeping costs down amidst the labor shortage. Since 2008, Robotiq has pursued its mission of freeing human hands from repetitive tasks by enabling more than 13,000 collaborative robots, or "cobots," worldwide. From SMEs to multinational companies, we're helping manufacturers simplify their processes with easy-to-use automation solutions.

Manufacturers want their operations to run smoothly with as little downtime as possible. Automation is often considered, but quickly dropped because of the perception that it is complex and expensive. At Robotiq, we tackle this challenge by making solutions that are actually easy to use. The Machine Tending Solution is the only solution you need to automate your CNC machines. Combined with our worldwide distribution network, you can automate a CNC machine in hours instead of weeks.

How can we back that bold statement?

The new version of Machine Tending Copilot was developed with the operator in mind. Cobots are simpler to use than industrial robots, but a machine-tending application is still complicated. For this reason, traditional programming can quickly get overwhelming. That’s why our Machine Tending Copilot software guides users through programming from start to finish. With key waypoints and action menus, programming is 75% faster than with traditional methods. Once the key waypoints are created, the user is guided to refine each operation with our action menus—from picking the workpiece to defining pre-programmed cleaning patterns . Since we know that every second counts in the manufacturing process, we’ve created the Smart Move. Using the Machine Tending Copilot algorithm, the robot finds the optimal path from point A to point B without colliding with the environment. This technology can shave up to 15% off your cycle time and shortens setup and downtime, which ultimately gets the machine up and running faster. Earn a quick ROI even with high-mix, low-volume automation; with accelerated program creation, Copilot does the hard work for you.

External modules manage communication with the machine interface, so there is no need to open or alter the machine in any way. This approach, which is similar to the way an operator would do the job, makes our solution compatible with almost all machine brands and models. We supply an external control box and pneumatic enclosure to accelerate installation.

Custom solutions can be costly and time-consuming to integrate, but the Machine Tending Solution takes less than two hours to deploy and machine your first part—no coding experience required.

Elevate your workforce with easy-to-use robot solutions that do the work for you.

COBOX - MACHINE TENDING SPECIALIST
App Kit
Cobot Planet

COBOX - MACHINE TENDING SPECIALIST

Flexible and straightforward process automation is a decisive factor in the drive to improve the productivity of your machine park and your employees. You can increase your competitiveness now with COBOX – a professional solution for quick integration with CNC machine tools. The workstation has been developed for trouble-free mounting of blanks in machine tool chucks and for removing machined workpieces. It is ideally suited for operating milling machines and turret lathes.
COBOX features a UR10e collaborative robot, a dual electric gripper and supplementary equipment depending on the configuration ordered – cobot base, frame, flexible workpiece handling and storage system (perforated plates with pins, gravity feeder or KLT containers), as well as a set of application-specific gripper fingers.
The centrepiece of the station is C-Interconnector – a PLC-based solution that enables seamless exchange of signals between COBOX and machine tools, as well as operation of all necessary functions in a plug-and-play manner. This, combined with the compactness of the workstation, enables it to be transferred between machines with little effort.
Two ways of implementation are available – as a complete ready-to-use CE certified solution with the implementation service package, including workpiece implementation support, training of staff and adjustment of machines, or on a do-it-yourself basis, where you can choose from the extensive range of components available in our online shop and assemble the workstation yourself according to the detailed instructions.

Humatics Milo Microlocation System
App Kit
Humatics

Humatics Milo Microlocation System

The Humatics Milo Microlocation System enables UR robotics to precisely interact with key assets external to the robotic arm in real-time enabling a new set of manufacturing automation applications to be delivered to improve productivity, quality, and profitability.

With Humatics Microlocation enabled alongside a robotic arm, you can accomplish highly precise tasks including in-motion assembly. The technology is well suited for the manufacturing environment enabling robotic arms to directly receive high fidelity positional data to take action on a moving part as it moves dynamically through a work space, such as a car chassis, an engine, etc., regardless of the lighting condition, clothes colors of workers, etc. The work cell becomes a digital ecosystem enabling a new class of robotic automation to improve productivity, quality and profitability.

Examples include:

  • Enabling robotic arms to accomplish in-motion assembly on an automotive final assembly line for improved productivity and quality. This includes engine bolt torquing, chassis bolt torquing, engine and chassis inspection, 7th axis tracking, etc.
  • General industry manufacturing lines that require the extraction of fixtured parts from pallets by robotic arms allowing for greater productivity and increased margins.
  • Enabling robotic arms that are placed on AMRs to become highly functional and precise in relation to the work they need to accomplish when the arm pulls up to a work zone on the mobile platform enabling the promise of a highly dynamic work cell.
  • In motion EV battery pick and/or placement from/to AGVs and AMRs, and battery placement and attachment to a moving chassis including aligning robotics to moving platforms.
  • Many more…

Local Office
  • Universal Robots USA, Inc
  • 27175 Haggerty Road, Suite 160
  • 48377 Novi, MI
Contact us: +1 844-462-6268
Contact us: + 1-844-GO-COBOT