str_len(str)
Returns the number of bytes in a string.
Please not that the value returned may not correspond to the actual number of characters in sequences of multi-byte or variable-length encoded characters.
The string is zero-indexed.
Parameters
str: source string.
Return Value
The number of bytes in the input string.
Example command:
str_len("Hello")- returns 5
str_len("")- returns 0