get_actual_joint_speeds()
Returns the actual angular velocities of all joints
The angular actual velocities are expressed in radians pr. second and returned as a vector of length 6. Note that the output might differ from the output of get_target_joint_speeds(), especially during acceleration and heavy loads.
Return Value
The current actual joint angular velocity vector in rad/s: [Base, Shoulder, Elbow, Wrist1, Wrist2, Wrist3]