set_baselight_iec()

Only applies to UR Series

Make the baselight comply to the IEC 60204-1 standard and indicate whether the robot is in a safety stop, in freedrive as well as the operational mode. Further details of the colors can be seen in the UR20 manual.