get_actual_joint_positions()

Returns the actual angular positions read by the joint encoders

The angular actual positions are expressed in radians and returned as a vector of length 6. Note that the output might differ from the output of get_target_joint_positions(), especially during acceleration and heavy loads.

Return Value

The current actual joint angular position vector in rad : [Base, Shoulder, Elbow, Wrist1, Wrist2, Wrist3]