get_joint_temp(j)

Returns the temperature of joint j

The temperature of the joint house of joint j, counting from zero. j=0 is the base joint, and j=5 is the last joint before the tool flange.

Parameters

j: The joint number (int)

Return Value

A temperature in degrees Celcius (float)