Tool I/O

Description

Tool I/O monitors and sets the live I/O signals from/to the control box.

 

 

To access Tool I/O

Tap Tool I/O on the left panel. You can see the editable fields of Tool Input and Tool Output on the right.

 

 

URCaps in Control drop-down menu

The Controlled By drop-down menu allows you to select a URCap that can control the tool settings. If a URCap is installed that has this capability, it will be displayed in the list. For instructions on installing a URCap, see URCaps.

 

When selected, the URCap will be responsible for the following settings:

  • Tool Output

    Setting can be 0, 12, or 24 V.

  • Dual Pin Power

    Setting is either true or false.

  • Domain for analog inputs

    Setting current/voltage per analog input, as seen in the pop-up when you tap one.

  • Power Output for digital outputs

    Setting Sinking/Sourcing/Push/Pull, as seen in the pop-up when you tap one.

  • Tool Communication settings

    These settings are not available on the user interface, but include enabled, baud rate, parity, stop bits, rx idle chars, and tx idle chars.

Upon selection of a URCap, any controls related to the above settings will be disabled. The new settings will be applied when an entry is selected in the drop-down menu, when the program is loaded, and when the program is played.