Unlock Safety Settings

Description

You have to unlock the safety settings to change them.

Safety Settings are password protected.

The default password for safety: ursafe.

 

Unlock safety settings
  1. In the PolyScope X Main Navigation, tap the Application tab.

  2. On the workcell screen tap the Safety icon.

  3. Observe that the Robot Limits screen displays, but the settings are inaccessible.

  4. Tap UNLOCK to make settings accessible, and enter the safety password.

  5. Tap Confirm, then Apply.

  6. Tap the Apply and restart button to confirm configuration to lock all Safety item settings again.