Lifting and Mounting g-Series
| Description |
This section describes how to safely lift and handle the robot arm. Proper lifting and mounting of the robot arm are essential for safe handling and to prevent equipment damage and personal injury. Follow the specified procedures when using lifting equipment, including a round sling, to maintain stability and control throughout the operation. The round sling is provided by UR with g-Series robots. Use it for lifting and handling the robot arm during transport, unpacking, and mounting.
|
|
Using a damaged round sling can result in injury.
Failure to secure the robot arm to a sturdy surface can lead to injury caused by the robot falling.
Incorrect assembly of components and/or wiring can lead to injury.
Installing or maintaining equipment connected to a power source can result in injury or death from electric shock.
Failure to use an appropriate lifting device for the weight of the robot can lead to injury and property damage.
Specific regulations for inspecting lifting equipment and for assembly lifting may apply in your region.
|
| Round sling specifications |
The round sling conforms to the following standards:
|
||||||||||
| Tilted mounting |
The robot arm can be mounted on a tilt from -180° to 180°. The most common positions are illustrated below.
|
| How to mount in tilted position |
To mount the robot arm at a tilt, follow these steps:
|