Adjusting the Password
| Description |
In the password settings in PolyScope X, you can find three different passwords.
It is possible to set the same password in all three instances, but it is also possible to set three different passwords to separate access and options. The default passwords are publicly available. To prevent unauthorized access, change the default passwords before operating the system or connecting it to a network.
|